2006-06-19 1:57 AM
2006-06-18 10:27 PM
Hi
I am using the USB bulk demo for IAR, thanks for all the people that have worked on this. I am having trouble getting it to work! When i run it on the STR711, when it links i get some errors, then when i connect the USB my PC says device not recognised and thaty a device connected to the USB has malfunctioned! I am using Win XP with all the latest updates. Any help would be much appreciated. Thanks2006-06-19 1:57 AM
Very silly mistake, the main function does not initalise any thing, (RCCU,XTI,EIC) added code and it worked fine, still get linking warning but dont think that it will cause any isues with the running of the project.
Thanks PhilWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.