2005-09-27 2:11 AM
2005-09-25 10:06 PM
Hi,
Is there some project ready to build for the IAR compiler? I tried to port the LCD example for the MB393 Eval board but I failed. (Well, I need a little time to know why, but driving the LCD isn't prior) Thanx Manu2005-09-25 11:24 PM
It seems that EWARM doesn't understand the
''inline'' in emi.h : error message inline void EMI_Config(u8 Bank, u16 Config) Error[Pe077]: this declaration has no storage class or type specifier D:\...\STR710_EVAL_LCD\include\emi.h 35 Is there any project option to rectify that ?2005-09-26 3:13 AM
In fact, IAR is not the problem
My problem is my JTAG debugger is an ione (from Isystem), so I have to use the winIDEA IDE to debug my projects. There are so many options that I don't control yet that I cannot to what I want. For example : i cannot compile a project under winIDEA in order to debug it whereas I can compile it under EWAR and I cannot download it to the microprocessor... i would have prefer my boss buy the RVDK toolsuite...2005-09-26 3:13 AM
In fact, IAR is not the problem
My problem is my JTAG debugger is an ione (from Isystem), so I have to use the winIDEA IDE to debug my projects. There are so many options that I don't control yet that I cannot to what I want. For example : i cannot compile a project under winIDEA in order to debug it whereas I can compile it under EWAR and I cannot download it to the microprocessor... i would have prefer my boss buy the RVDK toolsuite...2005-09-26 4:44 AM
For example this project compile with IAR IDE but cannot be tested (no Ione JTAG available in my toolchain)
and cannot be linked in winIDEA because I don't know how to tell the objects files xlink.exe has to link ________________ Attachments : STR710_EVAL_LCD.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1OC&d=%2Fa%2F0X0000000bmO%2Fl3xeR01E9_zBQ1dRQWw1BzU.wV3FyQne.mCRf_4rjpA&asPdf=false2005-09-26 5:34 AM
unfortunately no, it would be great because I have some project that compile in IAR IDE... and I spare my time trying to configure winIDEA...
2005-09-26 8:43 PM
OK, I can compile almost all my LCD project under winIDEA but I still have a problem with the linker xlink.exe :
--------------- Standard OUTPUT from linking. --------------- IAR Universal Linker V4.59O/386 Error[e46]: Undefined external ''?main'' referred in ?program_start ( D:\STR710_EVAL_LCD\Debug\71x_init.r79 ) 1 400 bytes of CODE memory (+ 57 992 range fill ) 6 144 bytes of DATA memory Errors: 1 Warnings: none --------------- Standard ERROR from linking. --------------- Maybe the lnkarm_ram.xcl isn't proper for my processor (str710F) / aplication?2005-09-26 10:30 PM
That's correct !
But what's the difference between ?main and main2005-09-27 1:48 AM
A ready to use project for winIDEA with IAR compiler toolsuite and Ione JTAG debugger.
Hope this will help the beginners with the same developpement chain. Manu ________________ Attachments : STR710_EVAL_LCD.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtIG&d=%2Fa%2F0X0000000aL9%2Fp7uXJKa8fqCk_Ghv9SGRj4OsrO.6X9_87rVkCVwlLbM&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.