2022-07-04 10:47 PM
How to debug those separated code via winIDEA.
Solved! Go to Solution.
2022-07-05 2:00 AM
Hello ,
Winidea seams to support SPC56 Families.
I recommend to create a separate program for z4d and z0h
you have an example on http://community.spc5studio.com (HAL Components Update Site)
SPC56ECxx OS-Less Z0 Slave Core Test Application
SPC56ECxx OS-Less Z4 Master Core Test Application
For this case , we have created 2 applications.
You can create with the same spirit 2 RLA applications (z4d and z0h)
Best Regards
Erwan
2022-07-05 1:35 AM
Multicore debugging is supported by UDE/PLS, our partner
If you are using WINIDEA, contact them to know if they are supporting SPC5xx multicore debugging.
Best regards
2022-07-05 1:46 AM
I have to create a single program for both the cores (core 1 : z4d and core 2 : z0h) or I have to create a separate program for z4d and z0h. Can you answer this?
2022-07-05 2:00 AM
Hello ,
Winidea seams to support SPC56 Families.
I recommend to create a separate program for z4d and z0h
you have an example on http://community.spc5studio.com (HAL Components Update Site)
SPC56ECxx OS-Less Z0 Slave Core Test Application
SPC56ECxx OS-Less Z4 Master Core Test Application
For this case , we have created 2 applications.
You can create with the same spirit 2 RLA applications (z4d and z0h)
Best Regards
Erwan
2022-07-05 2:18 AM
Thank you sir. I have one more doubt If i create separate program, Then how can I able to communicate the cores with each other
2022-07-05 11:01 PM
I couldnt get the sample codes for sample Slave core and Master core Test Application. Please guide me to get those codes. That website is not working...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.