2006-11-08 11:16 PM
2006-11-06 1:36 AM
Hello,
i inserted a a running code the IAP funtionality, (remapping ... based on the ST application). All works fine, except the SPI interface doesn't work anymore (works before). The BSPI1_CSR2 register is allways on state 0x00C4 (BERR = 1 and TUFL = 1) The IRQ vector is initialised with BSPI1IRQHandler IRQ_to_SYS ldr r0,=BSPI1_IRQHandler ldr lr,=BSPI1_IRQHandler_end bx r0 BSPI1_IRQHandler_end: SYS_to_IRQ in 71x_vect.s Has had anyone the same problem? or any idea? Thanks for help, Heribert2006-11-06 10:27 PM
Hello,
i want to rephrase my question: Is it possible to controll or check if the BSPI ISR is remapped right after starting the main application? Perhaps to look a a register in debugging mode? Thanks, Heribert2006-11-08 11:16 PM
Hello,
i insert the macro ''PERIPHERAL_INIT'' in the file 71x_init.s. (It is on default a comment line) Now work all the pheripheral systems ( in my case SPI) after a download of the main file. Don't ask me about the reason! Greeetings, HeribertWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.