2008-06-01 9:41 PM
2011-05-17 12:53 AM
Hello,
I found a mistake in IAP from ST in source:ymodem.c If the file is between 64K and 128K, the protection of sector1 is not diasbled -> you cannot write data in this sector. change the source in ymodem.c in Ymodem_Receive () as follws: else if (size <= 0x1FFFF) { /* Disable S0 and S1 write protection and erase them */ FMI_WriteProtectionCmd(FMI_B0S0, DISABLE); FMI_WriteProtectionCmd(FMI_B0S1, DISABLE);//This missing FMI_EraseSector(FMI_B0S0); FMI_WaitForLastOperation(FMI_BANK_0); FMI_EraseSector(FMI_B0S1); } Best regards2011-05-17 12:53 AM
Hello TRuf,
Yes, you are right. This is known and will be corrected in the next IAP release. Thank you. Best regards, Najoua.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.