2004-04-13 1:43 AM
2011-05-17 2:59 AM
Dear all!
Can anybody help me? I tried to used I2C and came across with one problem: I set SII, then I set STA bit (start condition), then I load S2DAT register and it sends this 8-byte serie. But after it, both SDA and SCL are in ''0'' state, while they need to be at ''high-impedance'' state. No device is connected to I2C from another side (uPSD3212 is the only device) and interrupts are disabled. Can we try I2C in such condition? Do you have any ASM-code exampple of I2C usage? Thank you in advance.2011-05-17 2:59 AM
We are working to release a uPSD3200 I2C driver that will be made available on our website (target release is within a month). A notification will be made on the forum when it is available.
On a case-by-case basis, a beta version of the I2C driver will be made available. If interested in receiving a copy of the beta version, please send a request tomailto:apps.psd@st.com
with the following information: Name Company Name Phone Number Location (City, State, Country) uPSD part number of device being used (3234, 3254, etc.) Application Projected annual volume (units) Regards, uPSD Applications EngineeringWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.