2004-09-22 4:17 AM
2004-09-22 1:26 AM
I have converted the str7 lib to gcc and have had no problems except with the I2C routines.
I have tracked the problem to the speed formula. If I use the datasheet formula the routines work all the time, with the lib formula the SB sometimes fails to clear after the address send. The I2C_SpeedConfig function uses the formula ((FCLK/Clock)/2)-7 to calculate the clock divider in the datasheet the formula is given as ((fPCLK1 / fSCL) - 7) / 2 which is correct ? The same also applies to fast mode. I have also just noticed that the FR2-FR0 are incorrectly set for speeds I2C_Init changes the value to the restet state of 0x20 but if you call I2C_FCLKConfig the value will not change. if (FCLK I2Cx->OAR2 |= 0x00; should be if (FCLK I2Cx->OAR2 &= ~0xE0; or set OAR2 to 0 in the init routine. Regards sjo [ This message was edited by: sjo on 22-09-2004 15:32 ][ This message was edited by: sjo on 22-09-2004 15:37 ]2004-09-22 4:17 AM
Hello, sjo
I agree with you concerning all your remarks; -In order to calculate the clock divider,I2C_SpeedConfig function msut sue the following formula ((fPCLK1 / fSCL) - 7) / 2 -For the second remark about the OAR2 it will be easier to set OAR2 to 0 in the init routine else all the I2C_FCLKConfig function has to be changed. Regards, HichWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.