2021-06-01 11:54 PM
i2c issue
i am using stm8s207m8t6 controller
i need 30 slaves and master
master side code ok
but issue in slave when initilize i2c
I2C_Init(300000, 0X30, I2C_DUTYCYCLE_2, I2C_ACK_CURR, I2C_ADDMODE_7BIT, 16);
if use 0x30 slave address slave respond.
if change slave address if any in 7 bit only slave not working.
out of 30 slaves only one save working 0x30 slave remaining all not respond
iam using STM8S_StdPeriph_Lib i2c two boards code
please help to solve this issue
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.