2006-05-31 12:13 AM
2006-05-25 9:39 AM
hi,
I use the communication between ST72F321 and memorie EEPROM 24c65 of microchip. all alone program I2C functions well in Reading & writing in the memory. but when I use interrupt Real Time Clock (RTC) [ MCCSR eo Timer B ], the bus I2C is frozen, I do not know why!? if you have an idea, pleaze help. thank you2006-05-31 12:13 AM
hi, i hope to have an unswer.
I'm going explaine now the program: i'm using GPS data via SCI bus, en then each 10 second we should store data GPS in I²C memory. the problem is when 10s is reached, i can't write to I²C data register ( I²C bus is frozen). N.B: i'm not using Active halt Mode, the MCU is in run mode.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.