cancel
Showing results for 
Search instead for 
Did you mean: 

I2C bus

lyeganeh9
Associate II
Posted on December 10, 2009 at 08:42

I2C bus

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
lyeganeh9
Associate II
Posted on May 17, 2011 at 15:02

I work stm8205k6 chip and i need to drive i2c bus

on standard mode & master mode.

power supply is 3v and fclk is 4.096 mhz.

can i2c bus drive with this supply?

I init GPIOB port to reset value at first

program.and use pull up resistor on SDA &SCL

lines but busy bit in the SR3 register always

set to 1 and not allow to do start condition!

it clear when swrst bit in CR2 register set

to 1.i don't know how to do!

i use ride7 IDE version 7.14

& Rkit-stm8 version 2.13.

bassinux
Associate II
Posted on May 17, 2011 at 15:02

Hello,

the reference stm8205k6 does not exist

for other questions :

The I2C can be drived by power supply 3V and Fclk 4Mhz

I advice you to use 4K7 ohm as value for pull up resistor

Best Regards

Bassinux

lyeganeh9
Associate II
Posted on May 17, 2011 at 15:02

Hi

thanks for your help

1.what does means ''reference stm8205k6 doesn't exist ''

don't i continue to work it and change my chip?

can i use the stm8207k6 chip?

2.I used 4K7 ohm resistor on SDA & SCL lines

but cannot drive i2c bus. my init i2c function

is in below:

{

I2C->CR1 &= ~(0x01); //disable PE

I2C->FREQR = 0x04;

I2C->CCRH |= 0x00;

I2C->CCRL |= 0x14; //fclk 100000hz

I2C->TRISER |= 0x05;

I2C->CR1 |= 0x01; //PE enable

I2C->OARH |= 0x40;

}

when send init function, busy bit set to 1.

then send start condition.but any happend on i2c lines!

bassinux
Associate II
Posted on May 17, 2011 at 15:02

Hi,

1) Regarding to the ST web site there is no chip with this name stm8205k6, the correct one is stm8207k6, this is which I mean by Reference.

2) Concerning your application it seems correct but I suggest to let the PE Enable the Last instruction.

After sending Start condition verify if SB flag in SR1 is set to 1.

be carefull in I2C pins mapping, verify if works with the correct package

Best rergards

Bassinux

lyeganeh9
Associate II
Posted on May 17, 2011 at 15:02

Hi

I checked the SB flag in SR1 register,

it isnot set to 1 after sending start condition.

i don't heve stm8s207k6 chip and still work with

stm8s205k6.is it possible 205k6 chip- i2c module

have problem?

thanks and best regards

lyeganeh9
Associate II
Posted on May 17, 2011 at 15:02

Hi

11 & 12 pin numbers(PB4 & PB5) are

SDA & SCL lines of i2c bus in the

stm8s205k6 chip (32 pins).

is it ok?

bassinux
Associate II
Posted on May 17, 2011 at 15:02

Hello I.yeganeh,

I suggest you to check the pinout.

brunomontanari9
Associate II
Posted on May 17, 2011 at 15:02

hi, the stm8s205k6 is the current STM8S105K6

regarding the problem, did you tested your application-hardware with the I2C example on the library? this is the quickest way to know if there is something wrong with your mcu. BTW, try using the 16Mhz configuration at first. I've had some issues when using the clock at 24Mhz

mathieux
Associate
Posted on May 17, 2011 at 15:02

Is this issue been resolved? I have the exact same behavior with the STM8S105K6. The SR3 Busy bit is always settled even if SCL and SDA pins are high level.

Thanks,

Mat

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.