2004-04-02 5:19 AM
2011-05-17 2:59 AM
Hello,
Someone could tell me if it is possible to use both I2C ports 1 and 2 of UPSD3234A but with different speed: - one at 100 KHz to accomodate old componants like SAA1064, - the other at 400 KHz to have communication with E2PROMS, Clock...2011-05-17 2:59 AM
Both I2C ports are clocked with the same programmable clock source so it is not possible to run one at 100KHz and the other at 400KHz.
Correction: Each I2C port has a SxCON register. There are three bits in this register that control the speed of the respective I2C port. Sorry for the mixup.[ This message was edited by: uPSD on 02-04-2004 17:49 ]2011-05-17 2:59 AM
You are correct. Sorry about the mixup.
2011-05-17 2:59 AM
Hello moderator,
I must disagree with you, I tested it and it works: the only difference between the 2 I2C apart of speed is that I2C-2 can be handled under interrupts, while i2C-1 not. void upsd_i2c_2_init (void){ P3SFS |= 0xC0; // Enable P3.7 for SCL, P3.6 for SDA S2CON |= I2C_400KHZ;// Setup I2C-2 for 400KHz (24 MHz XTAL) S2SETUP= STANDARD_HOLD_TIME_START_STOP; // 0x86 i2c_timeout_flag = 0; // clear timeout error flag IPA |= 0x02; // set high priority for EI2C IEA |= 0x02; // set EI2C I2C Int. Enable bit } void upsd_i2c_1_init (void){ P4SFS |= 0x03; // Enable P4.0 for SDA, P4.1 pour SCL S1CON |= I2C_100KHZ;// Setup I2C-2 for 100KHz (24 MHz XTAL) S1SETUP= STANDARD_HOLD_TIME_START_STOP; // 0x86 i2c_timeout_flag = 0; // clear timeout error flag // no interrupts for I2C-1 }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.