2019-03-26 3:06 AM
**To confirm connections, I did SWIM on STM8SDiscoveryKit and STM8S103FP6 breakout board & it worked well.
My board connections are as follows (STM8S Development Kit's Programmer ---> STM8S003F3):
VDD -> pin 9
SWIM -> pin 18
GND -> pin 7 (GND)
NRST -> pin 4
NOTE:
** Attachments below shows the error i get while trying SWIM interface on STVD & STVP.
Solved! Go to Solution.
2019-04-07 10:22 PM
Thank you for the reply , I've found the issue apparently ; I replaced my on board controller IC and it worked with same connection as i mentioned in my question.
2019-03-31 5:57 AM
Hi Nikhil!
If you want help, post some more info: schematics (is the SWIM pin free or something connected to it?), is the MCU not already programmed with pin RESET disabled?
Did you not plug the SWIM cable reversed? Are the jumpers ok set on your Discovery board?
Check all this and it will surely work!
2019-03-31 7:40 AM
Your MCU oscillator must be up and clocking to be able to go to SWIM mode
2019-04-07 10:22 PM
Thank you for the reply , I've found the issue apparently ; I replaced my on board controller IC and it worked with same connection as i mentioned in my question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.