2019-02-10 8:13 AM
Hi,
I'm using stm8s003f3p6 microcontroller and learn it's different internal peripheral. using SPL
How can i write a byte at RAM location like 0x00 and read from it.
i also want to use IAP commands for flash.
i have read stm8s Reference manual , dastasheet and flash programming manual, but i can't find related to.
do anyone has code example ,link or document or sample code.
Solved! Go to Solution.
2019-02-10 6:05 PM
uint8_t byte;
uint8_t* pbyte = 0x0000;
byte = *pbyte;
byte++;
*pbyte = byte;
???
2019-02-10 6:05 PM
uint8_t byte;
uint8_t* pbyte = 0x0000;
byte = *pbyte;
byte++;
*pbyte = byte;
???
2019-02-11 10:37 AM
Thanks,it worked.
Btw, im using Stvd , is there any other way(i mean without pointer) write value absolute memory locatiin??
Is stm8s memory(program memory, ram,eeprom) is bit addressable??
2019-02-11 11:06 AM
If you want to declare a variable at specific location, use specific compiler keywords, it should be in the compiler manual. (#pragma)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.