2019-05-20 2:32 AM
I'm using M95256 IC which is used as an external EEPROM for the controller. When i'm sending Read Status Register command i can see data from IC in receive buffer. But when i'm sending Read from Memory command, i get only 0xFF data in the buffer.I have checked the Status register after Write to memory command and the WIP = 0 and WEL=1 in the register. I'm not able to see the data on the oscilloscope as well even though i can see Read from memory command is getting transmitted in Tx Buffer as well as i can see it on oscilloscope.
2019-05-20 3:02 AM
Hello,
Please follow section 6.5 of datasheet attached.
Warning: Read operation can't be performed if a Write cycle is currently in progress.
Moreover, your status register value should be with WIP & WEL=0. I f WEL= 1 it means the write instruction didn't success.
0xFF correspond to the delivery state.
BR
EEPROM suPPort team
2019-05-20 5:16 AM
Hi,
My instructions sequence is:
1.WRITE ENABLE
2.WRITE STATUS REGISTER
3.WRITE DISABLE
4.READ STATUS REGISTER
5.WRITE ENABLE
6.WRITE MEMORY ARRAY
7.WRITE DISABLE
8.READ STATUS REGISTER
9.READ FROM MEMORY ARRAY
I have added delay of 5ms in between the instructions. But still the value of status register remains same i.e. WIP=0 and WEL=1.
2019-05-20 5:17 AM
Hi,
My instructions sequence is:
1.WRITE ENABLE
2.WRITE STATUS REGISTER
3.WRITE DISABLE
4.READ STATUS REGISTER
5.WRITE ENABLE
6.WRITE MEMORY ARRAY
7.WRITE DISABLE
8.READ STATUS REGISTER
9.READ FROM MEMORY ARRAY
I have added delay of 5ms in between the instructions. But still the value of status register remains same i.e. WIP=0 and WEL=1.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.