2017-01-06 5:57 AM
void main()
{ GPIOB-> DDR |= (1<<2); //output GPIOB-> CR1 |= (1<<2); //push-pull type output // GPIOB-> DDR &= ~(1<<7); //input // GPIOB-> CR1 |= (1<<7); //pull-up without interrupt GPIOC-> DDR &= ~(1<<2)|(1<<3); //input GPIOC-> CR1 |= (1<<2)|(1<<3); //pull-up without interrupt ///* Define FLASH programming time */
FLASH_SetProgrammingTime(FLASH_PROGRAMTIME_STANDARD);/* Unlock Data memory */
FLASH_Unlock(FLASH_MEMTYPE_DATA);/* Read a byte at a specified address */
add = 0x4000; val = FLASH_ReadByte(add);/* Program complement value (of previous read byte) at previous address + 1 */
val_comp = (uint8_t)(~val); FLASH_ProgramByte((add + 1), val_comp);/* Check program action */
val = FLASH_ReadByte((add + 1)); if (val != val_comp) { /* Error */// OperationStatus = 0; /* OperationStatus = PASSED, if the data written/read to/from DATA EEPROM memory is correct */ /* OperationStatus = FAILED, if the data written/read to/from DATA EEPROM memory is corrupted */ while (1) { } }}2017-03-06 2:26 AM
Thank you for your code !
It is helpful for the community.
Regards,
Simon
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.