2004-06-30 7:43 PM
2004-03-02 2:07 AM
I'm trying to program the st62t25c but never success , I mean that when i use it in the circuit it does not work. Of course i have tried the st62e25c for all the test and with this device every think works properly. Where I make a mistake?
GeB2004-03-14 9:16 PM
I've had also the same problem.
The reset vector is'nt correct. Look at the generated hex code at the last line! If there is'nt a reset vector, the assembler generated $FFh The stupid thing is, that the eprom version will works OK, but an OTP not!? How to solve the problem: Check your endline of your asm code. The END command must be followed by an ENTER command. I guess your reset vector is the last uC command So if there's no ENTER command after the END command, the assembler ignor the last uC command. Succes2004-06-30 7:43 PM
Hi , as suggested there may be a difference in the reset vector but this is not the root cause of your problem.
If you are using the linker ensure that section P1 is assigned correctly eg -P0:80-07ffWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.