2010-05-03 6:34 PM
How to implement microsecond delay on STM8S103F3?
2011-05-17 6:08 AM
How about the nop instruction approach ?
2011-05-17 6:08 AM
.ExternalClass0DCDBD5026184B978A5ED1ABAF097CF4 p.MsoNormal, .ExternalClass0DCDBD5026184B978A5ED1ABAF097CF4 li.MsoNormal, .ExternalClass0DCDBD5026184B978A5ED1ABAF097CF4 div.MsoNormal {margin:0in;margin-bottom:.0001pt;font-size:11.0pt;font-family:'Calibri','sans-serif';} .ExternalClass0DCDBD5026184B978A5ED1ABAF097CF4 span.EmailStyle15 {font-family:'Calibri','sans-serif';color:windowtext;} .ExternalClass0DCDBD5026184B978A5ED1ABAF097CF4 .MsoChpDefault {;} @page Section1 {size:8.5in 11.0in;margin:1.0in 1.0in 1.0in 1.0in;} .ExternalClass0DCDBD5026184B978A5ED1ABAF097CF4 div.Section1 {page:Section1;}
Hi
Boltnut,try this solution:
/* General Purpose 1µs Time base */
void Init_TIM2(void) { /* TimerTick = 1µs Warning: fcpu must be equal to 16MHz fck_cnt = fck_psc/presc = fcpu/16 = 1MHz --> 1 tick every 1µs ==> 1 µs / 1µs = 1 ticks */ TIM2_TimeBaseInit( TIM2_PRESCALER_16, 1); TIM2_UpdateRequestConfig(TIM2_UPDATESOURCE_GLOBAL); TIM2_ITConfig(TIM2_IT_UPDATE, ENABLE); TIM2_Cmd(ENABLE); } /** Wait a delay * @param[in] Delay based on timer Tick * @return None **/ void WaitDelay(u16 Delay) {GTimeStamp = 0x00; sim(); while (GTimeStamp <= Delay); rim(); }
/**
* @brief Timer2 Update/Overflow/Break Interruption routine. * @par Parameters: * None * @retval * None */ #ifdef _COSMIC_ @far @interrupt void TIM2_UPD_OVF_BRK_IRQHandler(void) #else /* _RAISONANCE_ */ void TIM2_UPD_OVF_BRK_IRQHandler(void) interrupt 13 #endif /* _COSMIC_ */ { GTimeStamp++;TIM2_ClearFlag(TIM2_FLAG_UPDATE); } Regards mozra
2011-05-17 6:08 AM
Can you explain what the sim()/rim() are in WaitDelay()
function ? My idea is shown as below:void I2C_Delay (u8 bTime)
{ /* ld a,(OFST+1,sp) 72 0007 0a01 dec (OFST+1,sp) 73 0009 4d tnz a 74 000a 26f9 jrne L13 */bTime /= 3; // 3.5 cycles each loop !
while (bTime--)
; } /* I2C_Delay */ bTime is in STM8S machine cycles (SYSCLK = 1 / 16MHz = 62.5 ns = 0.0625 us) !2011-05-17 6:08 AM
#define US(us) ( F_CPU / 3000000.0 * us )
#define MS(ms) US(ms * 1000) // maximum 10ms #define _delay( loops ) \ _asm(''$N: \n decw X \n jrne $L \n nop'', (U16)loops); #define _delay_us(us) _delay(US(us)) void _delay_ms( U16 ms ) { while (ms--) { _delay_us( 1000 ); } }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.