Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
HelloI'm using STM8S001j in my projectthe Project is simply an output on PB4 and output on PD6I needed to store in the EEPROM data every time the input is getting low I noticed that some times the data is recorded and some times not I monitored the E...
Trying to send an image but cannot.Please email or call and I can send the image.There are to many other images visible on the underside of the component (WLCSP) to confuse the vision system on the equipment. Even the equipment suppliers vision syste...
Because I don't find related information elsewhere (datasheet, application notes, etc.) I would ask it there.So, I have famous W1209 thermostat board with Nuvoton MCU, which I'm replace by an STM8S103F3.For proper operation it is needed to place an ...
I am using STM8AF5286 for one of my design. I am using CAN port for data transmission. I am using standard ST library for CAN communication. I don't see any 16-bit CRC calculation included in CAN_Transmit function of CAN driver function. Neither I se...
Hello to everyone, I am dealing with STM8S103F3P6 IC. I try to send a message using TX interrupt but I have never succeeded. I have checked the example of the UART interrupt. Also, tried to develop same code. However, I got still zero. I took interru...
Does anyone have the datasheet of the obsolete AIC33C93BL.I have attached the image of the component.Any response will be much appreciated, thank you.
After the STM8L152K6 device is programmed, it must be turned off and then on again for normal operation. However, if the STM8L152K6 device resets by pressing the Reset button after programming, it does not work. I have to do the power on reset once ...
I am (obviously) brand new to stm tools. I have installed the stvd and cosmic compiler and I want to use the firmware library. I have downloaded the STMS version. How do I install and use it? I've googled til my fingers are sore.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.