2018-02-16 11:18 AM
hi my name is mehdi . I'm using eDesignSuite for a Viper 27LN. how i choise transformer with Transformer Specifications?
Transformer Specifications:
fsw: 60 kHz - Isat ≥ 757 mA - Lp: 2.06 mH ± 10 % - leakage ≤ 3 % Primary: Ipk 617 mA - Irms 211 mA - Iavg 108 mA Aux: Ipk 189 mA - Irms 18 mA - Iavg 3 mA - Prim/Aux turn ratio 7.29 Out 1: Ipk 3.24 A - Irms 1.27 A - Iavg 750 mA - Prim/Out 1 turn ratio 7.76 Out 2: Ipk 3.24 A - Irms 1.27 A - Iavg 750 mA - Prim/Out 2 turn ratio 7.762018-02-19 1:53 AM
Hello Mehdi,
using VIPer27 flyback isolated design on eDesignSuite, a commercial transformer from Wurth should appear, if your specifications meet specific requirements. Could you please specify input and output values and if you have applied some customizations on your design?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.