Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8S003F3P6 is protected

Hi everybody,I am using the STM8S003F3P6 development board (little blue one bought from AliExpress) and I am trying to program it using ST-LINK V2 (also bought on AliExpress). I wrote the code using STVD and now I would like to program the MCU. I tri...

M41T83ZMY6F RTC Reports Half the Actual Time

I am working with the M41T83ZMY6F RTC (internal crystal version) in a project and I’ve encountered an unusual behavior: when I read the time via I²C, the RTC seems to count at exactly half the expected rate. For example, after one real second, the se...

shan by Associate
  • 427 Views
  • 3 replies
  • 1 kudos

Resolved! STM32H723ZG + DS8500 HART Modem → OCD pin always LOW (No Carrier) when interfacing with 2088 Pressure Transmitter

I am working on establishing HART communication using an STM32H723ZG Nucleo board, a Maxim DS8500 HART modem, and a 2088 Pressure Transmitter (4–20 mA + HART). Hardware Setup: STM32H723ZG USART3 → Debug to PC (115200, 8N1, no parity) USART6 → Conn...

Resolved! Is the LM311DT rail-to-rail?

As per subject, is the ST LM311DT rail-to-rail? Farnell claims that it is, but that's the only place that says it is, I can't find a definitive statement in the datasheet.(I have used the TI LM311, and that is not rail-to-rail. I need to handle input...

AndrewIC by Associate
  • 711 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.