2004-06-21 4:44 AM
Hive Based Registry for STPC SBC using WinCE
2004-06-02 3:23 AM
I have Developed a platform using WinCE for STPC x86 based SBC. When I change the Storage Registry from RAM based to Hive Based the plateform is not a bootable in SBC. Can anybody tell me about that metter? Is there any change required in the files. I take the tools from that available in WinCE4.2 version.
[ This message was edited by: AmitB on 02-06-2004 15:53 ]2004-06-21 4:44 AM
G'day
Check out the platform.reg. Do you have the right things in the hive boot section? As much I remember I had to do just some changes in [HKEY_LOCAL_MACHINE\init\BootVars]. The following stuff shut be in hive boot section: - [HKEY_LOCAL_MACHINE\init\BootVars] - [HKEY_LOCAL_MACHINE\Drivers\Resources\IRQ - [HKEY_LOCAL_MACHINE\Drivers\BuiltIn\PCI] - #include ''$(DRIVERS_DIR)\block\atapi\ALI1543.reg'' - #include ''$(DRIVERS_DIR)\block\msflashfmd\sdnpci\sdnpcid\sdnpcid.reg'' - [HKEY_LOCAL_MACHINE\Drivers\BuiltIn\Atapi] Does someone have some experience with putting the system.hv on a Static RAM instead the IDE- Drive? (in WinCE 4.2) Chris *** parts of platform.reg *** ; @CESYSGEN IF FILESYS_FSREGHIVE ; HIVE BOOT SECTION ; 2003-07-11: changes [HKEY_LOCAL_MACHINE\init\BootVars] ''SYSTEMHIVE''=''Documents and Settings\\system.hv'' ''PROFILEDIR''=''Documents and Settings'' ;''PROFILEDIR''=''Documents and Settings portrait'' ''Start DevMgr''=dword:1 ''DefaultUser''=''User'' ; : end of changes ; END HIVE BOOT SECTION ; @CESYSGEN ENDIF FILESYS_FSREGHIVE [ This message was edited by: chris_s on 23-06-2004 15:40 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.