2025-05-26 8:35 PM
What does the 'High' optimization actually do in IAR Embedded Workbench 9.60.3 when the 'Size' option is selected, but no additional optimization checkboxes are enabled. Even without selecting any extra options(like CSE, loop unrolling, etc. ), the code size reduces significantly—up to 30%. How is the IAR Embedded Workbench 9.60.3 achieving this reduction, and what specific optimizations are being performed in this case.
Solved! Go to Solution.
2025-05-27 12:07 AM
Welcome @Abdul_Aziz, to the community!
the IAR Embedded Workbench is a product of IAR, so this question can probably only be answered by someone from IAR, if they happen to be reading here.
But it would probably be better if you asked the support of IAR?
Regards
/Peter
2025-05-27 12:07 AM
Welcome @Abdul_Aziz, to the community!
the IAR Embedded Workbench is a product of IAR, so this question can probably only be answered by someone from IAR, if they happen to be reading here.
But it would probably be better if you asked the support of IAR?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.