Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What is the proper external ISR procedure to resume normal operation after entering halt mode on the STM8S?

First off, I would really like to thank everyone in the community for being so great. Second, I would really like to thank anyone who is willing to take a few minutes to read this post and answer my hopefully quick question. I am having a difficult t...

JEREMYB by Associate
  • 1442 Views
  • 1 replies
  • 0 kudos

STM8S208C6 wtih M24SR

Hy Guys,It is possible to use a STM8S208C6 microcontroller to use in conjunction with NFC / RFID M24SR64. Because I can not find any example software code for application for microcontrollers STM8S for NFC M24SR.

CPomm by Associate
  • 794 Views
  • 1 replies
  • 0 kudos

M41ST85WMX6TR contains an embedded 32.768KHz crystal, but it has not any crystal’s information in RTC’s spec or design note, so what's the crystal used in M41ST85WMX6TR? Or what's the embedded crystal's electrical parameter

M41ST85WMX6TR contains an embedded 32.768KHz crystal, but it has not any crystal’s information in RTC’s spec or design note, so what's the crystal used in M41ST85WMX6TR? Or what's the embedded crystal's electrical parameter

Wwang.11 by Associate II
  • 956 Views
  • 0 replies
  • 0 kudos

My design with HVLED001B does not work.

Hi all,Attached my design with HVLED001 does not work. If i replece HVSU resistor with 1kOhm starts to works and output is ok but IC temperature getting very high quikly abouve 100C degree. IC supply voltage is okey and about 17-18VDC. I can not whe...

ESaba by Associate
  • 1372 Views
  • 0 replies
  • 0 kudos

Equivalent microcontroller for STR912 series

Hi,The controller part number mentioned is obsolete now.Controller : STR912FAW47X6We are looking for new microcontroller were we can port the source code into the new one with no/minor changes. The Workbench details are also mentioned.CrossWorks for...

PMohan by Associate II
  • 844 Views
  • 0 replies
  • 0 kudos

About STM8AF VDD rise-time rate problem。

Page 12 of the STM8AF52xx STM8AF62xx Errata sheet mentions the power rise rate problem. the original written to : Nevertheless, we observed that Some very specific applications could have a VDD starting from a residual voltage already Above 0V and ...

ema by Associate
  • 763 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.