2023-04-11 3:57 AM
Usually the ST has a lot of documentation of their products. I also found few people also write in Internet that it is impossible to find any information about this ST product
If somebody can share more information about this IC
Solved! Go to Solution.
2023-04-14 12:39 PM
Welcome, @DS.5apoundjiev, to the community!
This device has long been obsolete, which is why no more information is available from STMicroelectronics for it. We are very sorry that we cannot help you any further.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
2023-04-14 12:39 PM
Welcome, @DS.5apoundjiev, to the community!
This device has long been obsolete, which is why no more information is available from STMicroelectronics for it. We are very sorry that we cannot help you any further.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
2023-04-14 2:00 PM
Usage suggests it's a custom part used by HP, so technical data probably isn't available to outside parties.
2023-04-16 11:35 PM
Thank you @Community member
I had some doubts that HP ordered this IC to STM, and STM designed and manufactured it.
2023-04-16 11:43 PM
Thank you @Peter BENSCH for the reply
but ti looks like there never been public documentation and the reason is not that the IC is obsolete.
There is also no new substitution of this IC.
At least is good to know that I have to speak with HP and not to STM. But because the ST name is on the IC I started to search and ask in STM direction.
Also, are you sure that this IC is obsolete at all, because HP uses it even today and many other companies also.(what are your sources of information, did you speak with colleagues, or you have some database with this info, or you were part of the dev team)
2023-04-18 2:21 PM
Yes, I am sure that the device produced by STMicroelectronics is obsolete. However, it is possible that it was something like an ASIC that was also produced by other manufacturers with the same number. But neither to other manufacturers, nor to the former device from STMicroelectronics is any statement possible, everything else would be speculation.
I am extremely sorry not to be able to give a more positive and pleasant answer.
Regards
/Peter
2023-04-19 2:09 PM
Thank you, Peter :thumbs_up:
2023-04-20 8:50 AM
You're welcome!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.