2026-01-29 11:04 PM - last edited on 2026-02-23 4:58 AM by mƎALLEm
Hello ST Community,
I am using HCF40106YM013TR in one of my products. One channel is configured with an RC timing network at the input, and its output is cascaded to another channel.
However, the output is chattering / oscillating near the positive trigger threshold voltage.
The RC values and operating conditions are as follows:
R = 500 KΩ
C = 4.7 µF
VCC = 14 V
GND is connected through a series diode for reverse polarity protection
The Schematic and output waveform also attached herewith FYR,
Wave form 1 : VCC (DSO channel 1) vs Capacitor charging (DSO channel 2).
Wave form 2 : Capacitor charging (DSO channel 1) vs HCF 10406 output (DSO channel 2)
Kindly suggest how to obtain a stable and smooth output and whether any changes in RC values, grounding, or protection scheme are required.
Thank you for your support.
Solved! Go to Solution.
2026-02-23 4:38 AM
Welcome @Yo1, to the community!
Your problem is caused by several interacting factors:
All together, these produce very unpredictable behaviour, which is also temperature-dependent.
To name just a few points:
Possible improvements:
Hope that helps?
Incidentally, it helps to get a response more quickly if community members don't have to go through the hassle of downloading and launching a PDF reader, but can see the relevant images directly in the thread when you insert them there using the camera button.
And one more thing: although taking a photo with your mobile phone is quick and easy, it will be blurry. However, your scope from GW Instek has a USB port below the screen that allows you to save screenshots directly to a USB stick. Screenshots like these dramatically increase people's willingness to help you!
Regards
/Peter
2026-02-23 4:38 AM
Welcome @Yo1, to the community!
Your problem is caused by several interacting factors:
All together, these produce very unpredictable behaviour, which is also temperature-dependent.
To name just a few points:
Possible improvements:
Hope that helps?
Incidentally, it helps to get a response more quickly if community members don't have to go through the hassle of downloading and launching a PDF reader, but can see the relevant images directly in the thread when you insert them there using the camera button.
And one more thing: although taking a photo with your mobile phone is quick and easy, it will be blurry. However, your scope from GW Instek has a USB port below the screen that allows you to save screenshots directly to a USB stick. Screenshots like these dramatically increase people's willingness to help you!
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.