2015-01-17 3:01 AM
Hello Friends,
I am working with STM8S to develop Remote Control.So, I want that my STM consume low power during halt mode & it will wake up based on GPIOC (switch) Interrupt.sw press = remote send on commandsw press = remote send off commnad...... I uses halt() function which is in <stm8s.h> library.During Run time (Continuous Work) = 20 mA Power ConsumptionAfter halt() function:During Halt mode = 10 mA Power Consumption.My Que are :->>>
only halt() function is enough to use ST in Halt Mode ? or any other Flag need to be set ?->>> How to maximum power consumption in STM8S (because 10 mA is too much) ? Thanks & Regards,HardipWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.