2008-02-20 6:07 PM
2011-05-17 12:49 AM
Hi,
I am trying to connect STR912 based target(self made PCB) board with Parallel Port Based Jtag hardware. This is first time I am working on STR9. I am unable to detect target device through H-JTAG. I am facing following problems.. I have kept TAP configuration as suggested in H-JTAG User Manual Fig 3-12 TAP Num – 0 IReg Len – 5 TAP Num – 1 IReg Len – Auto TAP Num – 2 IReg Len – 8 Iam getting device id as 0x12CB3020 When the TAP configuration is not done I got 0x02471E40 Both are invalid device ids. In site link a different TAP configuration is mentioned like this. TAP Num – 1 IReg Len – 5 TAP Num – 1 IReg Len – Auto TAP Num – 1 IReg Len – 8 I have not yet tried out this TAP configuration. Please let me know which is correct. Is Target Reset is must as shown in Fig:3-11. And also can I use nSRST instead of nTRST to reset target hardware for the figure shown in 3-11 of H-JTAG user manual as I do not have support for nTRST in my JTAG hardware. By seeing the change of Device ID received when TAP configuration is changed can I ensure chip is working to some extent. Please let me know how I could proceed further in these circumstances. Thanks in advance for the support,2011-05-17 12:49 AM
The device has been detected using the configuration
TAP Num – 1 IReg Len – 5 TAP Num – 1 IReg Len – Auto TAP Num – 1 IReg Len – 82011-05-17 12:49 AM
hi, rajugnv
have you succeeded to program either of the flash of STR91x with h-jtag? how to? thank you! best regards tsyejay2011-05-17 12:49 AM
NO. I could not. We are Using Keil ULINK to do it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.