2003-07-18 4:30 AM
2003-07-14 5:10 AM
Chaps,
I've been looking around the datasheets for details on the rising/falling edge interupts on the GPIO port. The Elite Programming Datasheet has registers for programming rising/falling edge interupts, interrupt unmask etc (section 13), but which interrupt is polled? I'm assuming it's a hardware interrupt. Anyone Known? Thanks. MurF2003-07-18 1:49 AM
It is a hardware interrupt but you have to enable and configure it using the chipset register (I/O in 0x22/0x23) number 0x58.
Bit 0-3 = IRQ number with some limitation (IRQ 0, 1, 2, 8 and 13 not possible) Bit 7 = 1 to enable the interrupt, 0 to disable For example: outp( 0x22, 0x58 ) outp( 0x23, 0x89 ) will enable and use the IRQ9 By default, this register is set to 0 and GPIO IRQ is disable. Farfalla [ This message was edited by: Farfalla on 13-08-2003 11:05 ][ This message was edited by: Farfalla on 13-08-2003 11:05 ]2003-07-18 4:30 AM
Most brilliant! Thanks Faralla. Will soon have my interrupts workin!
MurF.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.