2008-02-07 5:57 AM
2011-05-17 12:49 AM
Hi, I use the evaluation board REVA for ST microcontrollers. The ic include was the STR912F. I have a problem. I use some port like the #6 and #4 as bidirectional 16 bits bus. I use the gnu compiler and external circuit. My problem is that when I put the port in out mode :
SCU->PRR1 |= 0x00100000; // release P6 reset SCU->PCGR1 |= 0x00100000; // clock gating P6 SCU->GPIOOUT[6] |= 0x5555; //normal out for all pin GPIO6->DIR = 0xFF; // Dir output on GPIO6 for all pins -- -- GPIO_WRITEDATA(GPIO6, 0xF0); //work fine but when SCU->GPIOOUT[6] |= 0x0000; //input mode GPIO6->DIR = 0x00; // Dir input on GPIO6 for all pins var = (GPIO_READDATA(GPIO6)); There is a problem. The pin of the port #6 stay in output mode. They didn’t return in hiz mode. I couldn’t with the other ic bring the pin to other state. I try to put the port in read mode then in write mode and it work but once in write mode I can’t bring it back to release the pin in hiZ to let other ic on the bus to take control of it. The port ## 8 and 9 work. I just have to switch the dir register and the pin is release. The other ic can put there info on the bus. But with the port 0-7 the pin isn't release. Those port shoud be input and output. How can I put the pin in hiZ after put it in write mode. Can someone help me with that. Thank you for your help :-[2011-05-17 12:49 AM
Your statement
SCU->GPIOOUT[6] |= 0x0000; //input mode doesn't do anything. You need to also make sure none of the peripherals are driving the outputs (not just the GPIO).2011-05-17 12:49 AM
I try to just change the dir register but i didn't see any change in the pin. For the other device i didn't even release them of the reset mode register SCU->PRR1 and SCU->PCGR1. I just release the GPIO function. I try with all port and they do the same thing except for the port 8 and 9. When I switch the dir register they become Hiz state. So the other ic on the bus can drive the bus.
There should have a way to release the output and to let him return to Hiz mode(except to reset the ic). I try to return the port in resret mode then back to work but it didn't work. I'm sure somebody else had meet the same problem. Please help... :o2011-05-17 12:49 AM
I install the Ride version 7 and it solve the problem. i can now switch the port from output to input mode. There may have a bud on the version 6. When I install the version 7 the version 6 start to work ????.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.