2002-10-24 10:06 AM
Getting started with ST72521: C source example ?
2002-10-23 7:36 AM
Do you have any C source code to easily getting started with the ST72F521 ?
2002-10-23 9:00 AM
hello
i saw that you are from france so you could send me an email at this address:mailto:lpetrus@tekeleceurope.com
I call you back to help you for your new design with ST72F521. i look forward to your answer regards LP2002-10-24 10:06 AM
Refer to the ''ST7 Com library or app note'' discussion to know where to download application notes and software libraries. It will definitively help you getting started.
Now if you want, you can also use this ST72521 code shell that works with the Cosmic C compiler. It is loaded with comments so I believe you will like it. This code shell compiles code using gmake, the maker : that's a little bit more complex than a batch file but that's more powerfull. Be carefull with the makefile (file called by the maker, see appli.mak) since it makes the difference between space and tab. Make also sure you have the same Cosmic path as the one defined in the script file (see appli.lkf) and the makefile. Good luck for your project Jojo ________________ Attachments : 521_cs.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Bd&d=%2Fa%2F0X0000000bWA%2FjRZitKX4YPvxFRL40_kZpTFelOze3mRfxrSf84k9EeA&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.