2004-01-09 6:50 PM
Getting last ST6 tools (AST6,LST6,WGDB6)
2004-01-09 1:06 AM
I reseved a start kit that i bought. The software on the CD ROM is not the last release.
Can you help to find a way to download the last version of AST6, LST6 and WGDB6 tools ? Thanks.2004-01-09 3:25 AM
I can upload them if ST do not help, you can use the Raisonance toolchain with the starter kit aswell - its a much better tool to use.
These are the latest versions I have: AST6 - v4.50 LST6 - v3.40 WGDB6 - v2.8.0 Regards sjo2004-01-09 6:50 PM
The CD-ROM you got may have the previous versions of AST6,LST6 and WGDB6. Find attached the latest versions for AST6/LST6 and WGDB6(2.8.0).
These packages are no more available on the ST site because these are not supported now and has been replaced by the Raisonance tool chain. Like sjo, i will also suggest you to use Raisonance toolchain. Its better tool as it features a powerful macro-assembler, a linker, a C compiler and a state-of-the-art simulator and debugger. Its fully compatible with sources developped using the STMicroelectronics toolchain. Moreover, it supports all ST6 emulators: ST6xx-HDS2, Softec and CEIBO emulators. It is freely available(with only limitation of code size while writing code in C language) at www.stmcu.com/familiesdocs-html under Software Release section. ________________ Attachments : ST6_Toolchain.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0K3&d=%2Fa%2F0X0000000bXI%2FYESUKHjES7puHGkV.yHXuIJNmM0qSTpES93kSWXBonA&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.