2006-02-02 3:58 PM
Getting a PCM Output on uPSD3400
2011-05-17 3:10 AM
My attempts at getting a simple PWM output on TCM5 leaves me baffled.
My Keil code on a 24MHz uPSD3434E is:- PCACON1 = 0x00; // Disable PCA, use prescaled clock CCON3 = 0x14; // 1:16 prescaler, PCA clock enabled TCMMODE5 = 0x41; // fixed frequency PWM CAPCOMH5 = 0x80; // nominal 50% duty cycle PCACH1 = PCACL1 = 0; // zero the counter // Set P4.6 for TCM5 use P4SFS0 |= 0x40; P4SFS1 &= ~0x40; PCACON1 |= 0x40; // Enable PCA I am not seeing any activity on P4.6 so I have missed something, perhaps others can see my obvious mistake. To add a note: I assume interrupts are not necessary when operating the PCA for PWM output as all interaction is contained within the PCA hardware.2011-05-17 3:10 AM
To answer my own post - in another software module P4SFS0 was being cleared soon after the PWM setup - effectively returning the port pin to GPIO mode. No wonder there was no PWM activity.
Lesson learnt - adjust only those attributes that are applicable to the module which in my case is P4SFS0 &= ~0xC0 and not P4SFS0 = 0 as I had.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.