2010-03-15 4:40 AM
2011-05-17 1:00 AM
This is one of several FUQs (Frequently Unanswered Questions) to ST.
This (as explained in the newest Flash Programming manual) can be prevented by executing the following instructions: MOV r0, #0x40000 MCR p15,0x1,r0,c15,c1,0 The problem is that if these instructions are executed at any time except during the initialization the ARM throws an Undefined instruction fault. I have found that a delay solves the problem, one just have to be careful that the compiler does not optimise the code away. whh2011-05-17 1:00 AM
Hi ,
I have exactly the same problem. Is this problem solved ? Pls let me know.2011-05-17 1:00 AM
The presented code screams for the use of the volatile type.
2011-05-17 1:00 AM
Here is my code to erase sector7 from bank0. This code is compiled to execute in RAM.
When I execute the code step by step in my debugger (Keil JLINK) it works. Without debugger it never returns...void Erase(void){
volatile long Time_Out = 0;
volatile vu32 FMI_Sector = FMI_B0S7;
/* Write an erase set-up command to the sector */
*(vu16 *)FMI_Sector = 0x20;
/* Write an erase confirm command to the sector */
*(vu16 *)FMI_Sector = 0xD0;
/* Wait until operation compeletion */
while((!((*(vu16 *)FMI_Sector) & 0x80))&&(Time_Out < TIMEOUT ))
{
Time_Out ++;
}
*(vu16 *)FMI_Sector = 0x50;
/* Write a read array command */
*(vu16 *)FMI_Sector = 0xFF;
} regards Luc
2011-05-17 1:00 AM
Hi,
in the past i used STR912FA and i solved the problem in this way: void EraseSector(u32 Sector) { /*slowed down to write
la flash (FMI @48Mhz) */ SCU_FMICLKDivisorConfig(SCU_FMICLK_Div2); /* Clear */ FMI_WriteProtectionCmd(Sector, DISABLE); FMI_EraseSector(Sector); FMI_WaitForLastOperation(FMI_BANK_1); FMI_WriteProtectionCmd(Sector, ENABLE); /* Full speed (FMI @96Mhz) */ SCU_FMICLKDivisorConfig(SCU_FMICLK_Div1); } All FMI routine of ST Library are execute in RAM. In FMI_WaitForLastOperation disable PFQBC see errata __ramfunc u8 FMI_WaitForLastOperation(vu32 FMI_Bank) { u32 Time_Out = 0; /* Write a read status register command */ *(vu16 *)(FMI_Bank) = 0x70; /* Disable PFQBC (see Errata pag 5) */ SCU->SCR0 &=~0x1; /* Wait until operation compeletion */ while((!((*(vu16 *)FMI_Bank) & 0x80))&&(Time_Out < TIMEOUT )) { Time_Out ++; /* Time Out */ } /* Write a read array command */ *(vu16 *)FMI_Bank = 0xFF; /* Enable PFQBC */ SCU->SCR0 |=0x1; if (Time_Out == TIMEOUT) { return FMI_TIME_OUT_ERROR; } else { return FMI_NO_TIME_OUT_ERROR; } }I hope
it is
useful
Paolo2011-05-17 1:00 AM
Hi Paolo,
Thanks for response. It stil does not work. Erasing a sector from BANK0 is no problem, erasing a sector in BANK1 does not work, except step by step with JTAG debugger. Do you still use the STR912 ? I hate this device ! Kind regards Luc2011-05-17 1:00 AM
So much for an appropriate use of volatile.
The following would be a more consistent usage
long Time_Out = 0;
volatile vu32 *FMI_Sector = (volatile vu32 *)(FMI_B0S7);
/* Write an erase set-up command to the sector */
*(volatile vu16 *)FMI_Sector = 0x20;
/* Write an erase confirm command to the sector */
*(volatile vu16 *)FMI_Sector = 0xD0;
/* Wait until operation compeletion */ ... Or more effectivelyvoid Erase(void)
{
long Time_Out = 0;
volatile vu16 *FMI_Sector = (volatile vu16 *)(FMI_B0S7);
/* Write an erase set-up command to the sector */
*FMI_Sector = 0x20;
/* Write an erase confirm command to the sector */
*FMI_Sector = 0xD0;
/* Wait until operation compeletion */
while((!((*FMI_Sector) & 0x0080))&&(Time_Out < TIMEOUT ))
{
Time_Out ++;
}
*FMI_Sector = 0x50;
/* Write a read array command */
*FMI_Sector = 0xFF;
} >>Do you still use the STR912 ? I hate this device ! Life would likely be easier if you used the library code, or were more familiar with C and the tool chain.
2011-05-17 1:00 AM
Thanks for reply. It seems to be OK now.
>>Do you still use the STR912 ? I hate this device ! >>Life would likely be easier if you used the library code, or were more familiar with >>C and the tool chain. I use the library code. I made a *.lib and linked it in my code. The part 91x_FMI was compiled to be executed in RAM. This does not work. When I compile the 91x_FMI files separate and link it in my code, it does work. I have been programming devices for over 20 years in C. I use this toolchain for NXP LPC2470, SAMSUING S3C2440 without problems. PIC16, PIC32 is a pleasure to work with... And, no, I think my life would be easier if the erratasheet is a bit smaller ... So, lets say I do not hate this device, but I never gonna love it ! Thanks anyway LucWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.