2004-08-09 5:57 AM
2011-05-17 3:02 AM
Hello,
i was using UPSD3234A on my old project and use flashlink.I use the same programming interface (pullup resistors, serial resistors etc.)as DK3200 board (it has 5V technology) and now i will use UPSD3254BV that works with 3.3V. Will be there any differences that i must apply with programming interface to use flashlink to program UPSD3254BV. Regards2011-05-17 3:02 AM
FlashLink works with both 5.0V and 3.3V devices (it is specified for operation from 2.7 to 5.5V). Pull-up resistors connected to 5V on the 5V version will be connected to 3.3V on the 3.3V version of the device. The hardware interface is the same.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.