2005-07-26 1:54 AM
2005-07-20 2:40 AM
I am powering of the internal flash by setting
FLASHR->CR0 |= 0x8000; // set bit PWD And then going into LPWFI mode The datasheet is not very clear about turning the internal flash back on again. Does this happen automatically ? It would appear to be doing this, but I would just like to make sure. I currently only have the interrupt vectors in Ram and have no delay and it seems to power up ok. The core is only running at 32Khz which will make the cycle time ~32us which is longer than the 20us suggested delay before accessing Flash. Does anyone know if the flash is automatically powered back on? many thanks Ben2005-07-26 1:54 AM
Yes the internal flash automatically powers back on following a wakeup event (interrupt, wakeup, system reset).
As you stated the fact that you resume operation from the 32KHz clock, you don't need to insert an extra delay of 20us corresponding to the flash initialisation time. OliverWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.