2011-08-03 11:53 PM
When I use PA6,PD6 is EXTI_Trigger_Rising_Falling.When PA6 go H-->L, it generate interrupt, but When I keep PA6 still Low, and PD6 go H-->L, it not generate interrupt.
Please help me. void main() { CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_1); GPIO_Init(GPIOD ,GPIO_Pin_6, GPIO_Mode_In_FL_IT); GPIO_Init(GPIOA ,GPIO_Pin_6, GPIO_Mode_In_FL_IT); EXTI_SetPinSensitivity(EXTI_Pin_6, EXTI_Trigger_Rising_Falling); enableInterrupts(); while (1) { }; } /** * @brief External IT PIN6 Interrupt routine. * @param None * @retval None */ INTERRUPT_HANDLER(EXTI6_IRQHandler,14) { /* In order to detect unexpected events during development, it is recommended to set a breakpoint on the following instruction. */ if(GPIO_ReadInputDataBit(GPIOA ,GPIO_Pin_6)== RESET) Conut1_count++; else if(GPIO_ReadInputDataBit(GPIOD ,GPIO_Pin_6)== RESET) Conut2_count++; EXTI_ClearITPendingBit(EXTI_IT_Pin6); } Tks all2011-08-04 4:39 AM
2011-08-04 7:08 AM
Still can not. If any PD6 or PA6 Low, can not generate interrupt by other Pin, I checked all Pin Px6 the same problem.
Please help me!2011-08-05 3:53 AM
If you have PA6 high, can you can interrupt @ PD6 H-->L.
Thanks!2011-08-05 4:18 AM
Yes, I am sure, I use Stm8L152C6.
If all pin H is no problem, but when 1 Pin Low, not interrupt at other Pin H->L or L ->H Seems when 1 Pin Low, it will latch interrupt generator.I tested with all port the same , look like this MCUs not support. Best regardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.