2025-07-18 5:41 AM - edited 2025-07-20 7:46 AM
Hi All,
I am trying to get up and running the above hardware. I downloaded the software for the board, and we already use IAR compiler here. After compiling and downloading (via the STLink), the system runs the program just fine.
However, I just need to run the system with the onboard POT and it is not moving or energizing the motor at all.
I changed the 6step_conf.h file to POTENTIOMETER_INTERFACE = 1 and all others to 0. Nothing happens.
All the voltages to the board are perfect (running 70VDC to the board via a 7 amp programmable power supply).
All help would be greatly appreciated. This is my first intro into using the part. Time is very tight.
regards,
Charles
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.