2009-09-22 3:55 AM
2009-09-22 12:35 AM
Hi, I need to make a division of two longs so I used the application notes of asm math routines but even writing the same instructions as the example I get the following error:
***Demo.asm(2554): as1 : Error 54: Can't match Addressing mode ' sla {dividend+3} it seems that I can use this addresing mode to move values like ''ld X,{dividend+3}'' but I can't use a direct instruction like in the example, perhaps I made something worng in the declaration of values?, it's the following: WORDS segment byte at 200-27F 'ram1' .tempquot DS.B 4 ;4bytes .quotient DS.B 2 ; .dividend DS.B 4 ;4bytes [ This message was edited by: bernat on 22-09-2009 13:06 ]2009-09-22 3:49 AM
The SLA instruction can only operate on short addresses, i.e. addresses which are one byte long.
The assembler can't translate your instruction because there isn't an opcode for something like SLA $209 regards EtaPhi2009-09-22 3:55 AM
ok, thanks for the answer, then I will make it in a different way.
but this means that there is a mistake on that application note, someone should correct it.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.