2005-11-18 5:22 AM
Erase is not available on PROGRAM MEMORY for ST7FLITE10
2005-09-19 12:00 AM
I try to use APISample-Software as command-line programmer with ST7STICK. If I enable the ''-erase'' option, the error message above is the only result.
This is the part of the source, that seems to make the problem: ////////////////////////////////////////////////// // Erase a memory area. // becareful depending on the device and on the memory area to // process Erase may be unavailable BOOL Erase(const char *szAreaName) { int iReturn=0; unsigned long iAreaId; if (IsErasableArea(g_szPrgDevice, ''PROGRAM MEMORY'')) { if ((iReturn = EGetId(szAreaName, &iAreaId)) == 1) { iReturn = EEraseAll(iAreaId); } else { LDisplayError(''Unknown memory Area name''); } } else { char szErrorMsg[200]; sprintf(szErrorMsg,''Erase is not available on %s for %s'', szAreaName,g_szPrgDevice); LDisplayError(szErrorMsg); } return (iReturn==1); } Please help!2005-11-14 7:31 PM
Thank you for reply. But why do I get an error message if I try to reprogram a read protected device?
Regards ReneWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.