2017-11-07 10:47 PM
Hello. Is it possible to enable ROP in application? Let's say I transmit a command to MCU through UART and then MCU enables ROP. I am using STM8AF6223.
It is stated in PM0051 that 'readout protection is enabled by writing 0xAA in the ROP option byte'. But in
STM8AF6213/23/23A/26
datasheet [8.1 Option byte description], OPT0 (ROP[7:0]) -> '0xAA: Enable readout protection (write access via SWIM protocol) Note: Refer to STM8S series and STM8AF series 8-bit microcontrollers reference manual (RM0016) section on Flash/EEPROM memory readout protection for details.'Maybe it is possible to enable it without using SWIM protocol?Thank youWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.