Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Problem in struct on header file

Hi there!I put this struct in the header file of my code, i´m using Cosmic C compiler and STM8S207 microcontroller:typedef struct{ bool a0:1; //flutuação bool a1:1; //equalização bool a2:1; //automático bool a3:1; //fuga terra + bool a4:1; //fuga ter...

MGarb.5 by Associate II
  • 3382 Views
  • 2 replies
  • 0 kudos

Flash Controller BTU

Is it necessary to execute the flash controller instruction BTU of the ST10F269 out of internal flash or it can be executed from RAM or external memory.

Dilly by Associate
  • 1075 Views
  • 0 replies
  • 1 kudos

ERROR IN PROGRAMMING MANUAL?????????

hello sircan someone, help me with that "SUB SP,#$9 " ,with is mentioned in the LATEST PROGRAMMING MANUAL OF STM8S PAGE 151.if you write that in an even very 1line program, you have an errorCan't match Addressing mode ' SUB SP,#$9'is there a n er...

Resolved! hello sir i use the nucleo stm8s208rb with asembler language, so i start with the st visual develop and write even a small program l

hello sira very simple asembler program ,with a big problemits in ST visual develop , with the inside st assemblerthat simple program ldw X,#stack_end ldw SP,X PUSH $C SUB SP,#$02gives that error  Error 54: Can't match Addressing mode ' SUB SP,#$02'...

What is the minimum program content required for the evaluation board (STEVAL-ISA164V1) to communicate with ST_SMED_Configurator? Supplement: I am using STNRG388.

From the drawing of DocID28549, PIN22 of the evaluation board (STEVAL-ISA164V1) is described as UART_Tx and PIN23 is described as UART_Rx, but if you search for UART in the attached source file, PIN17 and PIN18 will be searched.Which part of the atta...

HKOBA.1 by Associate II
  • 1166 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.