2006-07-27 1:41 AM
2006-07-26 9:30 PM
Hi,
I am using DEV3 emulator. In my program I set bit 1 in MCCSR to 1 to enable Main Clock Output. The problem is that the frequency I measure on this pin is half the frequency I have set in the Debug instruments/MCU configuration box. If I set Fosc to 16MHz I measure 8MHz on the MCO pin, if I set Fosc to 8MHz I measure 4MHz. I checked this with ST7FDALI and ST7LITE. Is this the way it should be or not? Thanks2006-07-27 1:41 AM
Hi,
Main Clock Output is FCPU which is Fosc/2 (have a look to the clock managment block diagram). Then it is normal you get half the frequence you enter. This abswer also your PWM problem. Best regards LaurentWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.