2005-04-11 11:40 PM
2005-04-07 4:36 AM
Je dispose d'un STR710FZ2T6
Est ce que j'ai besoin d'un driver pour l'USB ou est qu il fonctionne sans? Meme question pour l'UART, le CAN et la SmartCard... Merci Dam2005-04-10 8:29 PM
hello
what i want to know is: do i have to use a component loke MAX232 for the UART at the output of the microprocessor? thanks2005-04-11 4:01 AM
and what for using USB, CAN, and SC? do they all need driver component?
DamWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.