2006-08-10 7:35 PM
Does anybody port uC/OS to Str710?
2006-08-09 7:09 PM
I have My Own STR710 develope board.
I follow the AN1710 from micrium to port uC/os to my board in RAM mode. But I confused that linking with STR710-RAM.xcl ,the board doesn't work. maybe timer0 doesn't work,because I add some test code in bsp_init() and it's work ok. It is not Task switching. the code in Bsp_Init() { ... BSP_IRQ_VECTOR_ADDR = 0xE59FF018; /* LDR PC,[PC,#0x18] instruction */ BSP_IRQ_ISR_ADDR = (CPU_INT32U)OS_CPU_IRQ_ISR; /* IRQ exception vector address */ BSP_FIQ_VECTOR_ADDR = 0xE59FF018; /* LDR PC,[PC,#0x18] instruction */ BSP_FIQ_ISR_ADDR = (CPU_INT32U)OS_CPU_FIQ_ISR; /* FIQ exception vector address */ BSP_UNDEF_INSTRUCTION_VECTOR_ADDR = 0xEAFFFFFE; /* Jump to itself */ BSP_SWI_VECTOR_ADDR = 0xEAFFFFFE; BSP_PREFETCH_ABORT_VECTOR_ADDR = 0xEAFFFFFE; BSP_DATA_ABORT_VECTOR_ADDR = 0xEAFFFFFE; BSP_FIQ_VECTOR_ADDR = 0xEAFFFFFE; ... } doesn't work. Could you tell me why?2006-08-10 7:35 PM
I have sloved it
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.