2007-04-23 12:19 AM
2005-06-27 4:42 AM
2005-06-27 6:56 AM
How are you trying to communicate? Are you using the SPI or the UART peripheral? Which baud rate would you like to select?
2005-08-09 9:07 PM
The st7538's communication distance is 4-6km
2005-08-28 11:12 PM
are you sure?
How do you measure this?2007-04-22 7:20 PM
Hi,
I see a distance of a few hundred meters but with two entities only. As soon as there are more entities on the same network I only get 10-20m. E.g. with 30 entities have a max distance of 15 meters. My system is based on 24VAC though, so maybe those values are different for 220VAC. Regards Reny2007-04-23 12:19 AM
Hi,
Thank you for using STMicroelectroinics products and website. This forum is dedicated to ST7 microcontrollers. You will get better support by contacting our technical support : http://www.st.com/stonline/domains/support/contact_support.htm Best regards LaurentWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.