2024-12-10 12:45 PM
We are implementing two TDA 7293 amplifiers in a Master / slave configuration, for a 35 watt, 30 kHz drive of a high frequency device that operates between 2.8 ohms and 7.1 ohms on the output pins (5.6 ohms to 14.2 ohms per amplifier). We have a couple of questions we want to get clarified:
2024-12-10 1:22 PM
1. This is an audio power amp , so its output goes close to +/- supply .
2. no.
3. 26dB is minimum gain for stability; so your circuit should use 26dB or more.
At lower gain setting oscillation might start.
2024-12-10 2:35 PM
Q.2:
You can calculate high freq. limits via slew rate introduced distortion.
F = S-R / 2*PI()* Vp-p = 10 V/usec / 6.28 * 80 Vp-p = 20 kHz
Or setting Freq = 30 kHz, max output non-distorted voltage = 53 Vp-p
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.