2003-11-25 9:33 AM
2011-05-17 2:57 AM
Hi!
I'm designing a PCB with a µPSD3212 - but want to be able to put a µPSD3333 as an option. A FLASH-Link Port for the µPSD is designed on the PCB. In addition to the µPSD3212 the µPSD3333 has a ''DEBUG''-pin. What to do with this pin to be sure, that I can use the debugging-features? What external hardware do I have to use for debugging? I have the 3200 developement-board and the FLASH-Link-Interface for the printer-port. May I use this for a µPSD3333 as well? Will I be able to archive debugging-features with this? Is there already a App-Note for the µPSD3333, that sums up the debugging-features? Thanks very much![addsig]2011-05-17 2:57 AM
Please see the attached, AN1724 , Conversion Guide uPSD3200 to uPSD3300. Also attached, Application note AN1763, has a section on KEIL'S uLink USB-JTAG Debugger used on uPSD33xx.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.