2006-09-05 2:50 AM
Debug information with JTAG Interface?
2006-09-03 10:36 PM
Hello,
i also have trouble to run the ''B-Programm'' after the IAP initialisation. My question: is it possible to view the initialisation and jump to B-MAIN via the JTAG-Interface in any way? (I see in program A the jump to B) Is it possible to view the B-program initialisation alone? Thanks for help. I use IAR and J-Link.2006-09-05 2:50 AM
Hello again,
the IAP Driver (--> Bootloder or B-Program) works fine with connected JTAG Interface and debug mode. I wrote the bootloader with start-and end-address, B-Programm is still in the flash. In standard mode (with or without)connected JTAG Interface it doesn't work. With connected JTAG Interface, after a reconnect the USB plug on the JTAG Interface it runs. Only programming B-Programm, so all works. Does anyone have an idea, what is wrong? Thanks HeribertWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.