2016-10-17 2:12 AM
Hi,
is it possible to specify Options bytes in source file ?I mean something similar to what I use with Microchip PIC18 (in .c files):#pragma config WDT = ON // WDT Enabled#pragma config WDTPS = 256 // Watchdog prescaler 1:256#pragma config CP0 = ON // Program memory is code-protected#pragma config IESO = OFF // Two-Speed Start-up disabled#pragma config FOSC = HS // HS oscillatoror with Microchip PIC16 (in .asm files): __CONFIG _DEBUG_OFF & _FCMEN_ON & _IESO_ON & _BOD_ON & _CPD_ON & _CP_ON & _MCLRE_ON & _PWRTE_ON & _WDT_ON & _HS_OSCI have found only one method yet, which is via STVD->Tools->Programmer->OPTION BYTEThis is very clumsy, I would like to provide customer a single .s19 file that contains everything.2016-10-17 3:50 AM
Hello,
the short answer is: no. More in details you can declare the otpion byte values as constants in the source code, but then you need a debugger/programmer that understands these special values at special addresses and know how to program them transparently for the user, and that's not the case for STVD as of today (ZAP can do that, but it's not included in the Free Special Edition package). Regards, LucaWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.