2010-01-07 2:01 AM
compiler error with STVD and Cosmic
2011-05-17 6:06 AM
Hello
I work with stm8s-discovery evaluation board. My Processor: ST8S105. Workspace: STVD and Cosmic compiler. I try to compile my project based on 16499.PDF and I Receive the following error: ----------- Project movment_watch - STM8 Cosmic - Configuration Debug ------------- Removing intermediate files ... Done! ----------- Project movment_watch - STM8 Cosmic - Configuration Debug ------------- Compiling main.c... cxstm8 -itslib -ifwlib +debug -pxp -no -l +mods0 -pp -i''C:\Program Files\COSMIC\CXSTM8_16K\Hstm8'' -clDebug\ -coDebug\ main.c #error cpstm8 C:\Program Files\COSMIC\CXSTM8_16K\Hstm8\mods0.h:0 FlexLM Invalid host main.c: The command: ''cxstm8 -itslib -ifwlib +debug -pxp -no -l +mods0 -pp -i''C:\Program Files\COSMIC\CXSTM8_16K\Hstm8'' -clDebug\ -coDebug\ main.c '' has failed, the returned value is: 1 exit code=1. movment_watch.elf - 3 error(s), 0 warning(s) I would be happy to accept a solution2011-05-17 6:06 AM
Quote:
FlexLM Invalid host
FlexLM is the licence manager - isn't it? Are you sure you have properly licensed your Cosmic?2011-05-17 6:06 AM
Hi
Yes, I have the licence. but I think I know whay I get ERROR it becose I get the licence on my computer and I try to build the project on anather computer. Does that make sence?2011-05-17 6:07 AM
2011-05-17 6:07 AM
Thank you everyone
Help very Itzik2011-05-17 6:07 AM
;) you can do it, but you can specify your network path
run the command regedit and in the HKEY_LOCAL_MACHINE>Software>FLEXlm License Manager folder create new file: - Value name: COSMIC_LICENSE_FILE - Value data: your server when you have the license Regards mozraWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.